Dear Sir.
Please help calculate the voltage divider resistance of EN pin cut-off voltage of LM53601
VDC_POC: 12V
The cut-off voltage is 6V. What is the resistance of LM53601 disable, R19 & R25 when the VDC_POC voltage is lower than 6V?
The cut-off voltage is 4V. What is the resistance of LM53601 disable, R19 & R25 when the VDC_POC voltage is lower than 4V?