Hi,
As shown in the waveform below, blue trace is Vin and yellow trace is OC1 pin. OC1 pin was pull up by a 10k resistor to Vin. OC1 is a open drain. Typically when Vin power up and no over current triggered (no load actually), OC1 should be high with a short delay follow Vin.
In the waveform below, OC1 delay 8ms than Vin. Is it a normal performance of OC1 pin delay 8ms?