This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMR16030: can lmr160303 output add 10000uF capacitor

Expert 4330 points

Replies: 2

Views: 103

Part Number: LMR16030

Hi team,

my customer want to add 10000uF capacitor on the output of LMR16030, input is 24V, output is 12V@1A.

i do testing on our EVM, result shows it can powe on normally, start up time is long(about tens of mS), so i am checking with you if there has some risk of add big capacitor on LMR160303?

Thanks.

Regards, Sunny

  • Hi Sunny,

    LMR16030 can works with 10000uF output cap, pls check below points:

    1. only use LMR16030S

    2.  increase softstart time over 50ms

    3. check loop stability over full temp range,

  • In reply to Andy Chen:

    Hi Andy,

    Ok, many thanks for your help.

    Regards, Sunny

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.