Other Parts Discussed in Thread: TPS2378EVM-602
Hi,
Could you please provide me reference circuit for TPS2372 isolation PD 51W application?
Also what is recommended transformer?
Best regards,
Tiger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you please provide me reference circuit for TPS2372 isolation PD 51W application?
Also what is recommended transformer?
Best regards,
Tiger
Hi Tiger,
In general the TPS2373-3 is recommended for isolated 51W designs whereas the TPS2372-3 is recommended for non-isolated 51W designs. However, if wanting to use the TPS2372-3 in an isolated design for 51W/19V, I recommend using the TPS2372-3 along with the power stage from the TPS2378EVM-602 which uses a 51W/19V power stage. The transformer from the TPS2378EVM-602 design can be used and is recommended.
Please let me know if having any additional questions. Thanks!
Best Regards,
Brett Colteaux
Thank you very much, Brett.
We will study them.
Have a nice day.
Best regards,
Tiger