Hello,
Customer is having a problem with the device:
input of 14V and an output of 1V at 1A.
I am unable to get more than 600mA out of the supply when I ramp up the load and unable to start the supply at all if the load is greater than 400mA. I copied the WebBench simulation that I generated at the time but when I try to simulate it now, I get different values. Virtually all of the components are different. Was it wrong? Why are they different? I also cannot run a simulation for this design now. I get an error of “Simulation not enabled for this design.”
What could be causing this issue?
Any comment on their questions regarding the webench?
Thanks!
Kevin