Other Parts Discussed in Thread: BQSTUDIO
Hi TI,
i have some questions regarding the correct implementation of the BQ35100 together with a battery type ER18505M LiSOCL2 3.6V.
I do not have an eval-board nor the bqstudio to begin with.
I wrote a small driver for the bq35100 to communicate with my mcu.
My application just switches on the device every hour doing some 2-3 minute task and shutdown.
I have currently used the EOS mode and i am reading the current, voltage, measruedZ, scaledR, temperature and SOH.
I left all settings in default just changed some minor things.
I do following:
switch on the modul via GE pin waiting
reading control register checking for INITCOMP to become 1 and for EOS_BAD_OCV, SOH_ERR and SOH_MERIT=0
setting in EOS mode via writing to appropriate flash registers.
starting the modul via GAUGE_Start cmd checking via control register
write away i start my application
after coming back i switch off bq35100 via GAUGE_Stop cmd takes a time until G_DONE and GA
after that i start reading the values and shutdown
But the SOH is at beginning rapidly went down than stabilize at a number. After doing a test over weekend the values became 0.
But for sure the battery is not empty at all i still use it until now.
Also if i track the resistor value i recognize they are not differing, so the stay the same over that period?
Thanks you in advance