Hi,
my assigned customer wants to use LM5119 in this configuration:
dual phase, Vin = 18V..60V, Vout = 12V, I_load_cont = 12A, I_peak = 16A
They tested the EVM and noticed, that the current in both phases differs a lot. Measuered with a eYinem RMS-Multimeter at the sense resistor of the FET, the discrepancy is 12%. Is there any material adressing current balancing? Or is there any tweak or process my customer can follow to change that?
Kind regards,
Marion