Other Parts Discussed in Thread: TPS54160
Dear Sir
Please help calculate TPS62160 EN pin cut-off voltage.
POC cut-off voltage between 5V and 6V. Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AJ,
TPS54160 is guaranteed to be disabled if EN is below 0.3 V. It is guaranteed to be enabled if EN is above 0.9 V. Your resistor divider will have 0.295 V at EN when VIN = 5 V. It will remain off. TPS62160 does not have a precision enable circuit that is programmable with respect to VIN.