Other Parts Discussed in Thread: UCC256301, UCC256402
Hello, we are currently developing 2kW AC/DC Rectifier. The output voltage is 43 ~ 56V and I am using LLC Converter to configure UCC25600.
The frequency range of ucc25600 is 40 ~ 350kHz, can the above output voltage range be possible?
The main output voltage is 54V and I set it to enter burst mode around 1A. However, as the voltage drops to 43V, the current entering burst mode increases, resulting in a waveform with output ripple entering burst mode.
Is it possible for the burst mode to go below 3A within the ucc25600's frequency range? Or should I change to an IC like ucc256301 with a wider frequency range?
Please review.
Thank you.