Other Parts Discussed in Thread: LMR33630
Tool/software: WEBENCH® Design Tools
Hi,
I now plan to using LM22670 for +12V@2A,-12V@1A when the input is 24V. But WEBBENCH can't support the simulaiton when the output is more than 5V.
Can the LM22670 Meet such application requirements?
In addition,when i want to simulate LMR33630 in WENBBENCH,but WEBBENCH is not available for the inverting usage of LMR33630.
looking forward for your reply.