Hello team,
Based on our requirements:
Vin: 6V - 12V
Vout: about 14V and Iout=140mA.
From calculations it should be around 47uH, but on the excel spreadsheet with this value I get as result the following suggestion: “Inductance outside tested range. User responsible for confirming control loop stability ”.
So I would like to ask you what it actually means, I can still use a 47uH using the stability calculations proposed on the file, or it is better to reduce the value of the coil?