Other Parts Discussed in Thread: LM5069, TPS2493, CSD19536KTT
I am having trouble with this evaluation board during high load conditions. Or application input is 42V DC and the input source can detect shot if startup current reaching near 32 Amps. To avoid that we would like to use this as an Inrush limiter. Our total output capacitance is 1067 uF and loads current is about 30 Amps. To increase the default sense current limit I changed R15 to 10ohms and R16 to 50ohms and R7 to 2mohms. The board is sufficiently able to limit the inrush but Mosfet starts smoking when load source about 30Amps also I noticed that Mosfet temperature is getting very high above 100C.
The other solution we tried is to use 3 parallel IRFH7085PbF power MOSFET on a new board with 1K resistor on the Gate and we are experiencing the problem as Mosfet in the middle starts getting hot and smoking at load condition.
Second Setup:
Please advise testing anything differently.
Thanks.