Other Parts Discussed in Thread: BQ76200, BQ76920
Hi, I'm getting started with a new battery management design. I am getting through a lot of the datasheet material and starting the schematic. I have a few questions. Here are a few details about my design:
1. We only need to monitor the cells and do balancing. I plan to use LTC7001 high side FET driver, so I'm planning not to use the CHRG/DISCH pins. I plan to use a dedicated microcontroller to read the status of the cells and determine when to break the circuit from charging. Is this okay?
2. I don't need the current sensing, is there any issue with leaving the sense pins floating? Or should I tie them to ground?
3. We plan to balance with only 20mA current, so I'm not planning to add external transitors. With 4.22V cell, I selected 105ohm resistors because there will be two of them in the discharge path, correct? So, 4.22V / (2*105) = 20mA. Ok?
4. I am mostly following figure 15 in the datasheet. I am confused by the little boxes near the cells that contain "VC10x" and "VC5x" respectively. Does this mean I should connect these nodes to the VC10x and VC5x pins? I think so, but not completely sure.
5. Could you quickly check the schematic so far? I found it sort of painful to follow the connections from figure 15, because I only have 12 cells. I think its correct, but wanted to check because some of the VC pins are shorted and it looks different from figure 15.
Thank you,