Hi support team,
how to calculate the value of R2 while UCC24612-1 in high side application
operation frequency 25K~65KHz
Vout = 12V/5A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Red,
It is recommended to set the RC pole formed by R2 and C2 to be 1/100 of the maximum switching frequency. Using equation 6 in the UCC24612 datasheet and with C2=1uF, R2 should be 1/(2*pi*1uF*65kHz/100) = 244Ω or greater.
Best Regards,
Ben Lough