This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 66
Part Number: TPS54116-Q1
Hello
I have a question about the LM541161-Q1.
What is the current limit value during the soft start period?
The current limit at Hiside appears to rise with the rise. (WEBENCH result)
Is there a calculation method?
Thank you.
Masazumi-san,
TPS54116 is a peak current mode controller.
According to the information on datasheet section 7.3.11, the part use COMP pin voltage to turn off the high-side FET. When peak siwth current intersect the COMP voltage, the high side switch is turned off.
During soft start, the COMP voltage rises up, that's why high-side current appears to rise.
Thanks
Qian