Hi
i want to pullup ILIM_HIZ pin with a resistor to 3.3v and config system from REG32[7]=0 and REG0x0F/0E in order to set current limit and also connect ILIM_HIZ to my host pin in order to be able to set it low when is necessary (because ILIM_HIZ pin as also related to HighZ mode)
my questions are:
1- is there any problem with design ?
2- what is difference if i leave ILIM_HIZ float ?
3- what is difference if i pull up with VDDA instead of V+3.3 ?
4- is there any contentious current to the pin (system is battery base and CT current is not good) ? is it too much?
5- how can i disable ILIM_HIZ pin ?
and about OTG/VAP mode pin i want to connect host and IC pins as below:
i need VAP mode because the load is a motor that can cause voltage picks when start and not interested in OTG mode.
as i understood from datasheet VAP mode is only when system is powered by batteries.
my questions are:
1- can i control VAP mode using this method?