Part Number: TPS22914
Other Parts Discussed in Thread: TPS22953
Hi TI experts,
I want to use load switch TPS22914 to direct continuous current from power supply to two loops.
The design circuit is as attached. I have a few concern regarding it:
1) Currents have to be bi-directional (some value between -2A to 2A). I want to make sure this part (without reverse current block/protection) can handle current in two directions.
2) The power supply is floating ground. How to limit Vin and Vout (referenced to the ground of the parts) to below the maximum rating?
I noticed that in the evaluation board, Vin is voltage limited and referenced to the ground. However, I'm current-limiting the current between Vin and Vout. I'm not sure how the part works for this 'current limiting' design.
3) Do you have any recommendations for choosing the value of C1, C2, and C3? In the case of current flowing in two directions, I would think they should be of similar value (~1 uF)?
Thank you in advance.
Yixin