Dear TI,
I have working with BQ24195 with following configuration, Here attached my Circuit, I am using Default Mode (without HOST mode).
From my circuit I did not use USB charging, so I have removed that section
I have short D+ & D- through R74, i did not install I2C pull-up(R76,R78) and Interrupt pull-up(R273).
I have not using OTG features so that pin directly connected to ground (through R280 0R) and CE pin also directly connected to ground(through ).
ILIM pin connected with 330R ( R282 ).
TS1 and TS2 shorted through (R274 and R276), R277 (5.23K ), R283 (30.1K).
I have above but STAT pin continuously blinking 1Hz.
Kindly Let me know if i made any mistake.
Is this ok for without host mode and how to debug this.
Thanks and Regards.