Other Parts Discussed in Thread: BQ24618
Hello, I want to use the BQ29700 device together with the BQ24618 charging controller.
So now my main question is if these components will works fine together?
Because the BQ24618 has still a lot of safety functions, I only need the Undervoltage Lockout function of the BQ29700.
For that reason, I only attached one MOSFET to the DOUT port. --> Is that ok for the BQ29700?
The BQ24618 has a battery detect feature --> Does the BQ24618 detect the battery if the MOSFET at DOUT disconnects the battery?
Now some questions to the BQ24618:
For the battery pack, I want to use 6x naked 18650 cells with 3500mAh, all connected in parallel.
Is it possible with the BQ24618 to set a precharge current of 1,8A --> 0,3A for each cell ?
What is the maximum precharge current?
What is the maximum current the BQ24618 can drive at the Stat1, Stat2 and PG outputs?
Would 14mA for each output be ok?
Thank you for your advice!