Other Parts Discussed in Thread: TPS61087, TPS61089, TPS61088
Hello,
I have a 12V motor that I need to drive from three 'C' cells; nominal total voltage 3.3V-4.5V. I see the EVM design is for 12V out, 2.65V to 5.5V, which is very similar. However, what would be the maximum output current for 3.3V to 4.5V input? Can I get 300mA or more?
Thanks,
Derek
P.S. I checked to see if this part is in Webench but I didn't see it there. Is there a very similar part I could use for Webench analysis?