Hi,
Based on the application below, is it possible to use a smaller inductor value like 2.2uH?
- VIN=5V
- Vout=12V
- Iout=0.75A
THanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Based on the application below, is it possible to use a smaller inductor value like 2.2uH?
THanks!
Antony
Dear Sir,
Please connect the fsw pin to Vin, then you can make TPS61087 work with 1.2MHz operation frequency. thus 2.2uH inductor is OK.