Hello Team,
I have some queries as mentioned below regarding TPS61322:
1)What is the continuous output current?
2)What is • the minimum switch peak-current limit that is mentioned in the datasheet?
Regards,
Mit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
I have some queries as mentioned below regarding TPS61322:
1)What is the continuous output current?
2)What is • the minimum switch peak-current limit that is mentioned in the datasheet?
Regards,
Mit
Hi MIT:
May I know you are asking for the data or the meaning of the short words?
For 1)What is the continuous output current?
I'm confused. May you explain the questions with more details?
For 2)What is • the minimum switch peak-current limit that is mentioned in the datasheet?
It's 0.5A for TPS61322.
Hi Mit:
Got it~
1)What is the continuous output current?
It means the current of the load in output side, and assume it's stable and continuous. (For example, connect a constant resistance at the output side)
2)What is • the minimum switch peak-current limit that is mentioned in the datasheet?
For the boost converter, the peak current is the current of the inductance. The converter will limit the peak value to protect the device. But the value will be varied by different condition such as temperature and manufacture, so that it will has the minimum, and maximum as tolerance.