Hello,
I would like to see the output ripple waveform on LM73606EVM with the following conditions:
Vin = 19V
Vout = 1.4V
Iout = 6A
Fsw = 400kHz
The datasheet provides output ripple at 3.3Vout only. Please also help with set-up picture while testing the ripple. Thank you for the help.
Regards,
Sanjay R. Pithadia