Part Number: BQ76920
Other Parts Discussed in Thread: BQ76200,
Hello everyone,
in my board, sometimes (I don' t know why and when), the SCD trigger ON! In my board there is 15x0.008ohm resistor in parallel, and when the false SCD triggered ON, it was about 120A and the Bq7692003 read 58.65mV. My SCD setup was: 150mV/400us and OCD: 100mV/160ms. I have a temperature sensor next the shunt and the mosfet. When the SCD triggered ON the temperatures were:
SHUNT:92°C
Mosfet:77°C
BQ7692003:62°C (sensor inside the Bq7692003)
Ambient: 49°C
I have a picture from oscilloscope, where the Yellow is DSG driver (from Bq76200), the light blue is the gate of discharge mosfet, the purple is the voltage on shunt, and the blue is the the Vpack voltage. Sadly, I the GND of probles of the oscilloscope don't were near the shunt resistor.
As you can see, the voltage on shunt never reach 150mV.
Some solution? Thank you in advance.