Hi,
We are currently using the LM5069 hot swap controller in the following attached circuit. We have made R44, the 0R resistor No Fit which is the only change so far. What we are experiencing is a failure of the device to turn on after it has been operating after approximately 30 on-off transitions over a period of a week. We have tested 7 of our hot swap controller boards and 2 have failed during normal operation.
We've gone through all the support components around the device and can't find an issue. It could be a transient causing the issue. What we have found is that on the failed units, the LM5069 is ignoring the fact that the over and under voltage conditions are fine, and Vin is at 48V.
We have measured that the GATE output is stuck at 0.6V when Vin is applied and does ramp to about 2.2V, then back down to 0.6V and stays there. Both failed devices have the same 0.6V DC voltage on the GATE output of the LM5069.
Do you know what could cause the LM5069 to fail and keep the GATE output, pin 10 at a constant voltage of 0.6V with Vin applied?
Best regards,
Patrick