Other Parts Discussed in Thread: TPS2121,
Hi,
IN1 : Main Battery (3 ~ 4.2v)
IN2 : Sub Battery (3 ~ 4.2v)
The sub_battery(IN2) is intended to be used for a while when the main battery(IN1) is removed or fully discharged.
PR1, OV1, OV2 and SEL are all connected to Gnd.
Currently, chattering occurs in either IN1 or IN2.
I think it's because of the comparator.
Is there a way to disable the comparison?
Thanks
Mark.Baek