Other Parts Discussed in Thread: UCC28881
The UCC28880 part is being used to supply power to a control circuit. The current design outputs 11V. Recently, the product this part is in has had several failures when the power is turn off then back on and the switcher stops operating. From what was scoped, the mosfet is no longer switching to provide output voltage. This failure can be repeated but does not occur every time. When the device is removed from AC for longer than 15 seconds then reapplied to AC, the IC will begin operating again. The measured values during failure: VDD=5V, FB=0V, HVIN to GND of the IC =160V with 120VAC input.