Deal all
I have question about error detection mode operates
Question
When current is controlled by internal S / W, error detection operates even in normal operation.
1. Current control: It can control from 0 to 65535 (16bit).
1) After setting the current control value to 39000 or higher, error detection operates.
-. LED is normal operates and Error detection is detected when SDO value is read.
-. Even if only one of the three parallel LEDs
2) If current control value is set as 65535 value, it will be detected unconditionally.
-. Even if 3 LEDs are in operation, error detection is detected when SDO value is read.
3) If the current control value is set below 39000, it operates normally.
-. Error detection is normal operate.
** Refer to below schematics
Thanks and BR
PJ