Other Parts Discussed in Thread: TPS74801, TPS7A83A, TPS56637
Hi all
My customer has this specification for an LDO: Vin=3.4V, Vout=3.3V, Iout=1A and he preselected the TPS7A7001.
Looking at the Datasheet I find this is marginal as the max dropout can be 200mV:
As they have a 5V on the board they could also use an LDO with VBias, however the TPS74801 doesnt seem to work here as Vbias-Vout > 3.25V
Can you suggest better options ? Would the TPS7A83A work ?
Best regards
Ueli