Hi!
I am facing a big problem with unstable voltage on the outputs.
I have got my converter calculated for 12V/3A on BUCK1, 7V/2A on BUCK2, and 5V/2A on BUCK3.
When there is no load all output voltages are correct. But when i try to drain more than 450-500mA from for example BUCK3 the converter starts to be ustable.
During unstable operation all voltages on the output drops and BUCK3 voltage looks like square wave.
I will try to put some load on other outputs as well but for know i need help.