This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 48
Part Number: UCD3138HSFBEVM-029
Tool/software: Code Composer Studio
Hi everyone,
I am using UCD3138HSFBEVM, i have refereed some videos in ti website, first thing is i have to write code for obtaing dpwm signals, i have attached code below.
I am not getting DPWM signal could you please tell me where am i going wrong?
#define MAIN 1 #include "system_defines.h" #include "Cyclone_Device.h" #include "pmbus_commands.h" #include "pmbus_common.h" #include "pmbus_topology.h" #include "variables.h" #include "function_definitions.h" #include "software_interrupts.h" #include "cyclone_defines.h" #include "stdio.h" #define PCLK_PERIOD 4.0e-9 #define PERIOD_SECONDS 10.0e-6 #define PERIOD_CLK ((int)(PERIOD_SECONDS/PCLK_PERIOD)<<4) #define EVENT1 (int)(PERIOD_CLK*0.00) int ram_event2; void inti_dpwm(void) { Dpwm0Regs.DPWMCTRL0.bit.PWM_MODE = 0; // Set to normal mode Dpwm0Regs.DPWMCTRL0.bit.CLA_EN = 0; Dpwm0Regs.DPWMPRD.all = PERIOD; Dpwm0Regs.DPWMEV1.all = EVENT1; Dpwm0Regs.DPWMCTRL0.bit.PWM_EN = 1; LoopMuxRegs.GLBEN.bit.DPWM0_EN = 1; } void main() { if(GioRegs.FAULTIN.bit.FLT3_IN == 0)// Re-Check pin assignment (ADC_EXT/SYNC may be?) { //clear_integrity_word(); } #if (UCD3138|UCD3138064) MiscAnalogRegs.CLKTRIM.bit.HFO_LN_FILTER_EN = 0; MiscAnalogRegs.CSTRIM.bit.RESISTOR_TRIM =23; //28; #endif //(UCD3138|UCD3138064) init_pmbus(0x58); init_dpwm0(); ram_event2 = Dpwm0Regs.DPWMEV2.all; for(;;) { pmbus_handler(); Dpwm0Regs.DPWMEV2.all = ram_event2; } }
Thanking you.
I don't see anything obviously wrong with it, except that you are calling init_dpwm0, and the function is called init_dpwm.
But I'm not a compiler or a UCD3138, so I'm not a very good judge.
Whenever I have to get a DPWM going, I start with an existing code, in this case, probably the lab codes which go with the videos, and change it from there, as quickly as I dare, which is often not very quickly, especially if the quick change doesn't work the first time.
That's the course I'd suggest for you.
Happy Debugging,
Ian Bower
In reply to Ian Bower:
Thank you for replying.