Hi Expert,
The customer's quality team is followed the datasheet's absolute maximum current ratings to judge the UCC28063 design.
Questions:
1) The DS is defined the ±25mA for Continuous gate current.But they can get the 50mA ~ 60mA RMS from the UCC28063 GDA&B pin directly.
2)The DS is defined the 20mA for Continuous input current of VCC pin.But they can see the VCC pin RMS current over the 20mA.
And the customer mentioned they can be measured from their legacy UCC28063 designs.
Pls advice us how to interpret the max current rating of UCC28063 VCC/GDA&B.
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E-Mail:Eric.Lai@ti.com