This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: Clock Trim

Part Number: UCD90160A


Team, 

My customer has the following question:

I have a few questions related to the UCD90160A that I could use some help with. Specifically related to the RUN_TIME_CLOCK_TRIM command.

 We are using the watchdog function in the UCD90160A device and my software team has informed me they've seen a fair amount of "error" on some devices (up to 2.5%). It seems the RTC trim command does affect the watchdog timeout. Can you confirm this is the case (ie is this actually trimming the internal oscillator)? Also when trying to use the SMBus debug tool to read/write this command, I'm seeing very different values read back from the device after writing a D8h command. Can you provide any clarification on the format of this command? 

Regards,

Aaron