Other Parts Discussed in Thread: TPS2546
Hi,
I want to recommend the TPS2547 to a customer who needs a USB charging and data transmit solution (capable of ID’ing if Apple and Android devices for charge control). He does not need/want variable voltage Power Delivery, just the 5V at up to 2.4A charging with ID. He will be using this with both a USB-A 2.0 connector, and a USB C connector, which will only have 2.0 data.
He tried to implement this previously with the TPS2546, but it was attached to a hub, and any time he went to attach a device for charging, it would disconnect ALL ports on the hub, causing a reset on other devices. After trying this with multiple hubs it had the same result.
My question is would the TPS2547 also have this issue? Is there a part you could recommend that does not have this issue with the same capability?
Thanks,
Lauren