HI Guys
Would CM322522-4R7JL inductor work for TPS61220 if max average current 50mA
Thanks
Rodney
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Guys
Would CM322522-4R7JL inductor work for TPS61220 if max average current 50mA
Thanks
Rodney
Hi Rodney:
Generally, it's recommended to choose a inductance with Isat>500mA. What's the Vin and Vout? And the 50mA means load current or input current?
To choose a proper inductance, we need to ensure it has enough value when facing the current spike. Not only considering stable status. The situations like load transient and the startup would take larger current than normal operation.
HI Munqiu
Thanks for the reply.
Vin: 3.2 - 3.7 VDC
Vout: 3.6 VDC
50mA load current (Actually only 20mA). 50mA would be max inrush
Thanks
Rodney
Hi Rodney:
We need to consider the worst case. Please ensure the inductance still has some capability for 400mA.