Hi expert,
May I know if UCC27282 can be configured as two low side driver to drive two N MOSFETs which are tided together on source?
That means, HS and VSS are connected in this kind of application?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
May I know if UCC27282 can be configured as two low side driver to drive two N MOSFETs which are tided together on source?
That means, HS and VSS are connected in this kind of application?
Thanks
Hello Sheldon,
Yes, the UCC27282 can work as two low side drivers, with the HS connected to VSS as you mentioned. The IC is tested in this configuration during some of the ATE tests and also bench validation.
Confirm if this answers your question, or you can post additional questions on this thread.
Regards,