Other Parts Discussed in Thread: PMP
Hi All,
I am new to SMPS design in general (although I have sucessfully designed a number of buck LED drivers)
I am looking to design a DC-DC converter to accept a wide ranging input for 14-160Vdc. Output can be fixed anywhere from 12V to 48V (I would prefer i higher voltage so 48V is optimum). The other main design driver is it has to be compact (PCB has no length constraint but PCB width can only be 14mm maximum and component height maximum 7mm)
After doing some pliliminary research I think the best topology for this design is SEPIC as the power is low, it needs to operate in buck-boost mode and by using a coupled inductor and only one MOSFET the component count (and footprint) can be minimised - although I am more than happy to go down a different approach if I'm wrong?
I have been looking at the TPS40210 and PMP6545 which shows a design that offers a 10-100V input and outputs 12V @1A.
From the schematic I understand that during start up the controller is powered from the input via D102, Q100 is only allowed to conduct whilst its source is less than around 8V due to the gate being supplied with 10V via R101 and D100. After startup the controller is then powered from the output. I am a little confused why Q2 and Q3 are required, they dont seem to be documented in the datasheet and are not used on some reference designs and are not on the EVAL board, can someone shed some light on this for me?
If i was to recreate this design would it be possible to just up grade the voltage rating of C2, C4, C6 and Q1 in order to change the input voltage range to 10-160V?
If I was to up grade the voltage rating of D1, C7, C8, C9 and change the value of R9 and R11 could the output voltage be adjusted to 48V?
Thank you for your advice,
Mark