This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 106
Part Number: TPS65381-Q1
Dears
user57070261. The actual measurement of this power supply. High current will cause TPS65381 breakdown of TPS65381 and damage the chip.Second, we want to reduce costs;
The experts on this device will reply to your question and propose some solutions, but I expect they will ask similar questions before they can propose a solution to your problem.
Thanks & Best Regards,
Brian
Find the right power solution for your processor or FPGA. Visit www.ti.com/SoCPower today!
Hello,
I want to make sure I understood your request. You want to replace the PMIC TPS65381 by simple LDOs and you need 2 rails 5V or 3.3V and 1.2V. What is the current consumption on each rail?
There is an option single device (TPS65320-Q1 or TPS65321-Q1) with 2 rails configurable BUCK + LDO. The quiescent current is very low i.e 100uA. Please check the specification and let me know if it fits your solution.
Regards
In reply to Mahmoud Harmouch:
Yes, you want to replace the PMIC TPS65381 by simple LDOs and you need 2 rails 5V or 3.3V and 1.2V. Three-output LDOs with car-grade requirements are required. The maximum input is 13V, and the output requires 5V / 1A, 3.3V / 500ma, 1.2V / 500ma, of which 1.2 and 3.3V are given to the periphery of the microcontroller and the core, to ensure that the core current is not less than 500ma.
Thanks a lot.
Elsa Duan
In reply to user5707026:
Hello Elsa,
LDO directly supplied from battery and 500mA, will cause huge power losses. The 3.3V LDO power losses is (13V - 3.3V)x0.5A = 4.85W. For this power you need a 5V step down BUCK and 2 LDOs supplied from the 5V. TPS65320 integrated LDO is only 280mA.
Replacing the PMIC TPS65381 by discrete solution may become more expensive and larger board space. The minimum discrete solution is:
- BUCK with input voltage Vbat = 13V and output voltage 5V. Should support at least 1.5A load
- LDO with input voltage 5V (BUCK output) and output voltage 3.3V. Power losses 0.85W
- LDO with input voltage 5V (BUCK output) and output voltage 1.2V. Power losses 1.9W
Regards, Mahmoud
We believe the question was answered and this post will be closed. Please open another thread for further question.