This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099EVM-768: .

Part Number: TPS61099EVM-768
Other Parts Discussed in Thread: TPS610981, TPS61099

HI TI, 

I have two questions

First,

I just got a TPS61099EVM-768.

I hope to make 3.3V output with 3.0V input. 

How can I make 3.3V output? Currently, it comes out with 5.0V.

If the evaluation board can not make 5.0V, is there any available EVB supporting 3.3V output with TPS61099x family?

Second,

I'm also looking at TPS610981. So, I want to compare two boosters.

If TPS610981 is compared with TPS610994, can you tell me which one will be better?

My application uses 10~70uA for long time, but sometimes it goes 45mA.

So, I'm thinking using the low power mode of TPS610981.

Thank you in advance.