Other Parts Discussed in Thread: TPS3808
Hello,
I need to use the TPS3840 with more than 10V of power rail input to monitor (to detect ~5V of that), but the max input voltage of the TPS6840 is 10V. Is it okay to use voltage divider circuit with very high resistance(to reduce current consumption) for VDD? How much current should be needed in order to operate TPS3840 without any issues?
Or would you advise a different device with similar parameters to the TPS3840?
Thanks,
Adam