Hi Experts,
- I would like to use a diode for clamping at the EADC, illustrated below. Is it ok? Will it be hazardous to UCD?
ps. I need only 0~0.6V sense range, but input voltage may have max 2.5V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
- I would like to use a diode for clamping at the EADC, illustrated below. Is it ok? Will it be hazardous to UCD?
ps. I need only 0~0.6V sense range, but input voltage may have max 2.5V.
you can use a voltage divider to scale down the input signal. The measurement range of EADC is 1.6V, but 2.5V will not damage UCD.
Hi Bosheng sir,
- But I don't want to use a voltage divider, since that will decrease the resolution.
- Is it OK to put a diode there?