Dear Sir, please answer
I made calculation using WBdesign for TPS610995. Please, see attach.
Please, report, can I use this circuit for input voltage range 3 - 4.2V ?
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir, please answer
I made calculation using WBdesign for TPS610995. Please, see attach.
Please, report, can I use this circuit for input voltage range 3 - 4.2V ?
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by
Hi Vladimir:
Please allow me double check with you firstly.
The input/output information is different between your post and the document attached. So what's the input rang, Vout, and load condition?
Dear Minqiu, thank you
1) I made calculation using WBdesign for TPS610995 for Vin = 1.75 - 2.4 V, Vout= 3.6V, Iout= 20 mA (for 1-cell lead acid battery), please see attach.
2) I also need power supply for Vin = 3 - 4.2 V, Vout= 3.6V, Iout= 20 mA.
Please, answer, can I use the the same circuit (in my attach) for Vin = 3 - 4.2 V ?
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by
Hi Vladimir:
OK, so you have two project same time...No wonder it confused me.
1. OK, the calculation looks well.
2. If the Vin>Vout, the TPS61099 will enter into down mode and passthrough mode. In down mode, the Vout could be regulate still as 3.6V. But in pass-through mode, it can't regulate Vout anymore.
So it's depends on what you expect when Vin>Vout.