My customers asks:
I interpret from the datasheet for the TPS74201, Vbias >= Vout + 1.62.
So for 1.2 Vout you need Vbias >= 2.82V and for 1.0 Vout you need Vbias >= 2.62V. If Vbias is 2.5V then Vout should be 0.88V .
I am not 100% sure is that the requirement or that is just a test condition for their measurements.
The second row says Vbias = 2.375 (min) without any conditions…
I am investigating if this LDO can make the same output voltages (1.0 and 1.2) with 1.5V input and 2.5V bias voltage.
Can you please confirm?