Dear team,
Nice to contact to you, I got a LP55231 with symptom from customer R&D.
All the process is provided as below,
1.Turn on chip (register 01h bit[6])
2.Turn on charge pump (register 36h bit[4:3])
3. Set PWM at 255 (register 16-1B) to 11111111
4.Set current at 175 (register 26-2B) to 10101111
5.Set PWM at 0 (register 16-1B) to 00000000 Or Set current at 0 (register 26-2B) to 00000000.
When I set register 16-1B or 26-2B to 0 one by one, LEDs are off all the time. I can still read register setting at this time, but LED cannot turn on no matter by setting register 4 or 5, register 16-1B, and register 26-2B until re-turning on power.
Do you have any advice for us to check the IC’s status when LED off happens?
Schematics as below, we use 3ch for one LED. In our system, total 2 LP55231 and 5 LEDs.
Thanks.
Kane