My system was observed to have a noise problem when the input voltage was raised from 12V to 24V. After some looking around, I observed a switching anomaly in the 3.4V supply using an LM5165.
The following is a trace of the switch node, with Vin=12V. The frequency was expected to be 400KHz based on Rt=51.1K (not 180KHz as observed), but that discrepancy is not a big problem.
The problem is that when Vin=24V, the single pulse divides into 3, creating much more noise in the system.
The following is the schematic:
What can I adjust to prevent this from happening? Output is 3.4V at about 110mA.
Thanks for any help, Michael