Hi Sir,
may i have your support to review TPS2372-4 schematic as attached? this is the application for 802.3bt. if have any problem or suggestion please kindly let me know,thanks for your great help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
may i have your support to review TPS2372-4 schematic as attached? this is the application for 802.3bt. if have any problem or suggestion please kindly let me know,thanks for your great help.
Hi Tommy,
DT5 and DT6 should be bidirectional TVSs as a PSE can provide opposite polarities.
I recommend considering a common mode choke in series with L4 and L6. Since this is a high power application, a choke will probably be needed.
R26 seems low. It should probably be 50k.
Lastly, I highly recommend using the PG signal to help delay the load when the PSE provides power to the PD (unless you already have a delayed load). This will help with interoperability where the PSE doesn't hit it's inrush current limit spec.
Hi Darwin,
thanks for your great support,
as for the delay load, PG pin must be connected to the converter SS pin? may i connect to enable pin?
Hi Tommy,
Yes you can connect to an enable pin of a DCDC as well to delay the load. Thanks!
Hi Darwin,
sorry~i have another question,
in addition to the SS pin method, if there is no DCDC, the output is +48v directly,
are there other circuit that can do delay load? do you have any related information or idea to share on hand? thanks.
Hi Tommy,
Usually, the load is controlled by a microcontroller. So the microcontroller will keep the load in a low power state until after 80ms.
However, in some cases this must be done through hardware in which you can use an SVS (with a delay capacitor) sensing the PG pin to create a delay. Then you can you use this delayed signal to drive the enable pin of a load switch or a high voltage hotswap that connects to the load.
Regards,
Darwin