Hi,
I have one problem now.
The problem is that the output voltage rises during the BOOST START period during startup, but the input current flowing during this period is large.
I want to lower this current value.
One way is to lower the value of BOOST_INITIAL_VOLTAGE as much as possible. Then it has been confirmed that the current value drops.
So, the question is, the VF of the LED is 20V in total, is it possible to set the value of BOOST_INITIAL_VOLTAGE to 20V or less? For example, 16V.
In this case, disable BOOST OVP.
If the above is not possible, I would like to take a different measure. Is there any other way to reduce the input current?