Part Number: BQ27220
Hi,
I have created this golden image for the battery monitoring (please find attachment) for my device which is supposed to work for prolonged period with a battery percentage feature. While testing I noticed that the Battery percentage reading that I get from the configured gauge drops by many values from 24 % to 7% in one of the examples I have monitored.
Please could you help me out as to what I have done wrong and how I can correct it.
The following is the reading that my device reads from the gauge every 5 minutes.
[2020-02-19 10:37:23.527] [I] GAUGE READ SUCCESS: 24 Percent 3610 mV 0 mA 23C
[2020-02-19 10:42:23.183] [I] GAUGE READ SUCCESS: 7 Percent 3609 mV -5 mA 23C
[2020-02-19 10:47:23.235] [I] GAUGE READ SUCCESS: 7 Percent 3609 mV -5 mA 22C
[2020-02-19 10:52:23.280] [I] GAUGE READ SUCCESS: 7 Percent 3609 mV -6 mA 22C
[2020-02-19 10:57:23.327] [I] GAUGE READ SUCCESS: 7 Percent 3595 mV -394 mA 22C
[The attached file was with a .fs extention, in order to upload I changed it to .zip. Please change the extension as you prefer]
Regards,
Noel.