This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Kazuto,
We do not recommend shorting the BATFET with this part. If you would like to put a System Load on the battery, that is fine. However, please make sure that the SYS and BAT pin are not shorted together.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.
Kazuto,
If you directly connect the System Load to the BAT pin, you will need some other way to distinguish the charging current from System Load. In addition, with this method, your system will have the same voltage as the battery. This means if your battery is depleted, the system will have the same voltage and may not be able to be powered up.
This part has the Narrow VDC architecture, which is the reason why the SYS and BAT pins are separated by the BATFET. In the event of a depleted battery, the SYS pin is regulated to the Minimum System Voltage (MINSYS) to allow the system to turn on. When the battery reaches MINSYS, the battery voltage is lower than the system by the VDS of the BATFET; the SYS voltage then begins to rise with the charging of the battery.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.