Hi team,
I would like to know the load current at which MODE change from PWM to PFM.
I understand it depends on Vin/Vout/Fsw and inductance of the coil, so here is my conditions below.
Vin = 24V and 28V
Vout = 5V
L = 2.2uH
Mode : AUTO
It is also helpful if you can share the equation to get the boundary condition.
I think the PFM starts when the load current decreased to the level at which the device starts DCM operation.
If there are other condition, please let me know.
regards,